Motor_Start_Delay
Motor_Start_Delay
| Address: | 8762 (223AH) |
| Type: | DWORD |
| Access: | Read/Write |
| Unit: | µs |
| Range: |
0 to 231 |
| Default Value: | 0 |
| Store Supported: | Yes |
| Description: | It defines the delay on the motor start. This object can be used to have repetitive motor starts. Each time the motor has to start (MOVE command executed, or Motor_SYNC object written or Trigger Start input detected) Motor_Start_Delay microseconds are waited. |
| Notes: | This object should not be used together with Motor_Start_Delay_Pulses object. |